Real Time

Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description

Channel Setup (Advanced LTE-A Pro FDD Uplink)

UL-SCH (E-UTRA)

UCI (E-UTRA)
UCI (eMTC)

UL-SCH (eMTC)

UL-SCH/UCI (NB IoT)

1. General Settings

Physical Channel Number

Displays the identifying number of the selected channel.

Name

Displays the name of the selected channel.

UCI = Uplink Control Information

UL-SCH = Uplink Shared Channel

Name (NB IoT)

Displays the name of the selected channel.

UL-SCH = Uplink Shared Channel (NPUSCH Format 1)

UCI = Uplink Control Information (NPUSCH Format 2)

State

Choice: Off | On

Default: Off

Double-click or use the drop-down menu to turn the selected channel off or on.

UCI Parameters: If the total number of antennas is set to 4 under the Uplink Cell Parameters, the state is set to off and is read only.

Power

Range: -60.000 to 20.000 dB

Default: 0.000 dB

Enter a power level in dB for the selected channel. See Output Power Calculation (Uplink) for a description of how the software applies your power setting.

Scrambling

Choice: Off | On

Default: On

Double-click or use the drop-down menu to turn scrambling for the physical channel on or off.

RNTI (UCI Parameter Only)

Range: 0 to 65535 (0x0000 to 0xFFFF)

Default: 1 (0x0001)

Enter the Radio Network Temporary Identifier (RNTI) for the corresponding PUCCH transmission.

The input method can be in decimal format or hexadecimal format.

Example: The decimal input "15" is displayed as "15 (0x000F)" and the hexadecimal input "0xf" is displayed as "15 (0x000F)".

See 3GPP TS 36.211 and 36.321, for more information.

RNTI (1)

Range: 0 to 65535 (0x0000 to 0xFFFF)

Default: 1 (0x0001)

Enter the Radio Network Temporary Identifier (RNTI) for transport block 1 (codeword 0).

The input method can be in decimal format or hexadecimal format.

Example: The decimal input "15" is displayed as "15 (0x000F)" and the hexadecimal input "0xf" is displayed as "15 (0x000F)".

See 3GPP TS 36.211 and 36.321, for more information.

RNTI (2)

Range: 0 to 65535 (0x0000 to 0xFFFF)

Default: 1 (0x0001)

Enter the Radio Network Temporary Identifier (RNTI) for transport block 1 (codeword 1).

The input method can be in decimal format or hexadecimal format.

If the "number of codewords" parameter is 2, this parameter is displayed. Otherwise it is hidden.

Example: The decimal input "15" is displayed as "15 (0x000F)" and the hexadecimal input "0xf" is displayed as "15 (0x000F)".

See 3GPP TS 36.211 and 36.321, for more information.

RNTI (NB IoT)

Range: 0 to 65535 (0x0000 to 0xFFFF)

Default: 1 (0x0001)

Enter the Radio Network Temporary Identifier (RNTI) for transport block 1 (codeword 0).

The input method can be allowed the decimal format or hexadecimal format.

Example) The decimal input "15" is displayed as "15 (0x000F)" and the hexadecimal input "0xf" is displayed as "15 (0x000F)".

See 3GPP TS 36.211 10.1.3.1 and 36.321 7.1, for more information.

Transmission Mode

Displays the transmission mode for the corresponding PUSCH transmission.

The Transmission Mode is dependent on the Total Number of Antennas used.

Transmission Mode 1 is used for single antenna transmission and Transmission Mode 2 is used for multi-antenna transmission.

1 : Single Antenna Port (Port 10) Default when 1 Antenna is selected under Uplink Cell Parameters

2 : Single Antenna Port (Port 10) / Closed Loop Spatial Multiplexing Default when 1 or 4 Antenna(s) is(are) selected under Uplink Cell Parameters

See 3GPP TS 36.211 and 36.213, for more information.

2. MTC Settings

Number of Subframes Scrambling Stays Same (N_acc)

Displays the number of consecutive absolute subframes over which the scrambling sequence stays the same (N_acc).

1: CE Mode A

4: CE Mode B

See 3GPP TS 36.211 for more information.

PUSCH Transmission Span (N_PUSCH_abs)

Displays the number of consecutive subframes including invalid subframes where the UE postpones the PUSCH transmission for BL/CE UE.

This parameter is used only when UE Type is set to BL/CE.

See 3GPP TS 36.211 for more information.

PUSCH Absolute Subframe Number (i_0)

Range: 0 to 10239

Default: 0

Enter the absolute subframe number of the first UL subframe intended for carrying the PUSCH.

This parameter is used only when UE Type is set to BL/CE.

This parameter should be set to a valid subframe number defined by Valid Subframes. Otherwise, an error occurs during the generation.

See 3GPP TS 36.211 for more information.

Number of Repetitions (UCI)

Range:

1 | 2 | 4 | 8 | 16 | 32: CE Mode A

4 | 8 | 16 | 32: CE Mode B

Default:

1: CE Mode A

4: CE Mode B

Double-click or use the drop-down menu to select the number of repetitions.

This parameter is used only when UE Type is set to BL/CE.

See 3GPP TS 36.211 for more information.

Number of Repetitions (UL-SCH)

Range:

1 | 2 | 4 | 8 | 16 | 32 for CE Mode A

1 | 4 | 8 | 16 | 32 | 64 | 128 | 192 | 256 | 384 | 512 | 768 | 1024 | 1536 | 2048 for CE Mode B

Default: 1

Double-click or use the drop-down menu to select the number of repetitions.

This parameter is used only when UE Type is set to BL/CE.

See 3GPP TS 36.213 for more information.

Guard Period

Choice: First 0 Symbol and Last 0 Symbol | First 0 Symbol and Last 2 Symbols | First 1 Symbol and Last 0 Symbol | First 1 Symbol and Last 2 Symbols | First 2 Symbols and Last 0 Symbol | First 2 Symbols and Last 2 Symbols

Default: First 0 Symbol and Last 0 Symbol

Double-click or use the drop-down menu to select the guard period.

This parameter is used only when UE Type is set to BL/CE.

See 3GPP TS 36.211 for more information

Narrowband Index for PUSCH (n_NB)

Range:

1.4 MHz: 0

3 MHz: 0 to 1

5 MHz: 0 to 3

10 MHz: 0 to 7

15 MHz: 0 to 11

20 MHz: 0 to 15

Default: 0

Enter the narrowband index. Available number of this parameter is determined by the system bandwidth setting defined in the Uplink node.

This parameter is used only when UE Type is set to BL/CE.

See 3GPP TS 36.211 and 36.212 for more information.

Resource Indication Value (RIV)

Displays the resource indication value (RIV).

This parameter is coupled to RB_START and Length of allocated resource blocks.

This parameter appears only when CE Mode is set to Mode A.

This parameter is used only when UE Type is set to BL/CE.

See 3GPP TS 36.213 for more information.

Length of Allocated Resource Blocks

Range: 1 to 6

Default: 6

Enter the length in terms of contiguously allocated resource blocks (L_CRBs).

This parameter appears only when CE Mode is set to Mode A.

This parameter is coupled to RB_START.

This parameter is used only when UE Type is set to BL/CE.

See 3GPP TS 36.213 for more information.

RB START

Range: 0 to 5

Default: 0

Enter the start resource block (RB_START).

This parameter appears only when CE Mode is set to Mode A.

This parameter is coupled to L_CRBs.

This parameter is used only when UE Type is set to BL/CE.

See 3GPP TS 36.213 for more information.

Allocated RB(s) within a Narrowband

Choice: 0 | 1 | 2 | 3 | 4 | 5 | 0 and 1 | 2 and 3

Default: 0

Double-click or use the drop-down menu to select the allocated RB(s) within a narrowband.

This parameter appears only when CE Mode is set to Mode B.

This parameter is used only when UE Type is set to BL/CE.

See 3GPP TS 36.213 for more information.

Frequency Hopping Flag

Choice: On | Off

Default: Off

Double-click or use the drop-down menu to turn PUSCH frequency hopping for BL/CE UE on or off.

This parameter is used only when UE Type is set to BL/CE.

See 3GPP TS 36.213 for more information

PUCCH Transmission Span (N_PUCCH_abs)

Displays the number of consecutive subframes including invalid subframes where the UE postpones the PUCCH transmission for BL/CE UE.

This parameter is used only when UE Type is set to BL/CE.

See 3GPP TS 36.211 for more information.

PUCCH Absolute Subframe Number (i_0)

Range: 0 to 10239

Default: 0

Enter the absolute subframe number of the first UL subframe intended for carrying the PUCCH.

This parameter is used only when UE Type is set to BL/CE.

This parameter should be set to a valid subframe number defined by Valid Subframes. Otherwise, an error occurs during the generation.

See 3GPP TS 36.211 for more information.

2. NPUSCH Settings

NPUSCH Format

Choice: 1 | 2

Default: 1

Use the drop-down menu to set NPUSCH Format Type.

Format 1: Used for data transmission. (UL-SCH)

Format 2: Used for control information transmission. (UCI)

See 3GPP TS 36.211 10.1.2.3 and 10.1.3 for more information.

Subcarrier Spacing

Choice: 15 KHz | 3.75 KHz

Default: 15 KHz

Double-click or use the drop-down menu to set Subcarrier Spacing.

See 3GPP TS 36.211 10.1.2.1 for more information.

Number of Subcarriers in Resource Block

Displays Number of Subcarriers in Resource Block.

See 3GPP TS 36.211 10.1.2.1 for more information.

Number of Subcarriers in Resource Unit (N_RU_sc)

Choice: 1 | 3 | 6 | 12

Default: 12

Double-click or use the drop-down menu to set Number of Subcarriers in Resource Unit (N_RU_sc).

This parameter is only selectable when NPUSCH Format 1 and Subcarrier Spacing is 15 kHz. Otherwise automatically decided with read-only.

See 3GPP TS 36.211 10.1.2.3 for more information.

Subcarrier Offset in RB (n_sc)

Choice:

0 (N_RU_sc = 12 and Subcarrier Spacing = 15 kHz)

0 | 6 (N_RU_sc = 6 and Subcarrier Spacing = 15 kHz)

0 | 3 | 6 | 9 (N_RU_sc = 3 and Subcarrier Spacing = 15 kHz)

0 to 11 (NN_RU_sc = 1 and Subcarrier Spacing = 15 kHz)

0 to 47 (Subcarrier Spacing = 3.75 kHz)

Default: 0

Double-click or use the drop-down menu to set Subcarrier Offset in RB (n_sc).

See 3GPP TS 36.213 16.5.1.1 for more information.

Number of Resource Units (N_RU)

Choice: 1 | 2 | 3 | 4 | 5 | 6 | 8 | 10

Default: 0

Double-click or use the drop-down menu to set Number of Resource Units for NPUSCH (N_RU)

See 3GPP TS 36.211 10.1.3.6 and 36.213 16.5.1.1 for more information.

Number of Repetitions (N_Rep)

Choice: 1 | 2 | 4 | 8 | 16 | 32 | 64 | 128

Default: 0

Double-click or use the drop-down menu to set Number of Repetitions (N_Rep) for NPUSCH.

See 3GPP TS 36.211 10.1.3.6 and 36.213 16.5.1.1 for more information.

Number of Slots in Resource Unit (N_UL_slots)

Displays Number of Slots in Resource Unit (N_UL_slots).

See 3GPP TS 36.211 10.1.2.2 for more information.

Number of Consecutive Slots for RV Index (B)

Displays Number of Consecutive Slots for RV Index (B).

See 3GPP TS 36.213 16.5.1.2 for more information.

Number of Consecutive Transmission Slots (N)

Displays Number of Consecutive Transmission Slots (N).

See 3GPP TS 36.213 16.5.1.2 for more information.

Number of Mapping Slots for NPUSCH (N_slots)

Displays Number of Mapping Slots for NPUSCH (N_slots).

See 3GPP TS 36.211 10.1.3.6 for more information.

Number of Repetitions of Identical Slots (M_NPUSCH_identical)

Displays Number of Repetitions of Identical Slots for NPUSCH (M_NPUSCH_identical).

See 3GPP TS 36.211 10.1.3.6 for more information.

3. MIMO Settings

Number of Layers

Choice: (Dependent on the Total Number of Antennas.)

1 (1 Antenna case) Default =1 when 1 Antenna is selected under Uplink Cell Parameters

1 | 2 (2 Antennas case) Default =2 when 2 Antennas are selected under Uplink Cell Parameters

1 | 2 | 3 | 4 (4 Antennas case) Default =4 when 4 Antennas are selected under Uplink Cell Parameters

Double-click or use the drop-down menu to select the number of layers for the corresponding PUSCH transmission. The number of layers is less than or equal to the number of antennas.

Number of Codewords

Choice: Dependent on the Total Number of Antennas and Number of Layers.)

1 (1 Antenna case) Default when 1 Antenna is selected under Uplink Cell Parameters

1 (2 Antennas, 1 Layer case)

2 (2 Antennas, 2 Layers case) Default when 2 Antennas are selected under Uplink Cell Parameters

1 (4 Antennas, 1 Layer case)

1 | 2 (4 Antennas, 2 Layers case) Default =2 when 4 Antennas are selected under Uplink Cell Parameters

2 (4 Antennas, 3 Layers case)

2 (4 Antennas, 4 Layers case)

Default: 1

Double-click or use the drop-down menu to select the number of codewords for the corresponding PUSCH transmission.

See 3GPP TS 36.211, 36.212 and 36.213, for more information.

Codebook Index

Range: (Dependent on the Total Number of Antennas, Number of Layers, and DCI Format.)

N/A (DCI Format 0 case) Default when 1 Antenna is selected under Uplink Cell Parameters or when DCI Format is set to Format 0.

0 to 5 (2 Antennas, 1 Layer case)

0 (2 Antennas, 2 Layers case) Default when 2 Antennas are selected under Uplink Cell Parameters

0 to 23 (4 Antennas, 1 Layer case)

0 to 15 (4 Antennas, 2 Layers case) Default when 4 Antennas are selected under Uplink Cell Parameters

0 to 11 (4 Antennas, 3 Layers case)

0 (4 Antennas, 4 Layers case)

Enter the codebook index for the corresponding PUSCH transmission.

In case of DCI Format 0, N/A is displayed.

See 3GPP TS 36.211, 36.212 and 36.213, for more information.

DCI Format

Choice: (Dependent on the Total Number of Antennas, Number of Layers and Number of Codewords.)

Format 0 (1 Antenna case) Default when 1 Antenna is selected under Uplink Cell Parameters

Format 0 | Format 4 (2 Antennas, 1 Layer, 1 Codeword case) Default =4 when 2 Antennas are selected under Uplink Cell Parameters

Format 0 | Format 4 (4 Antennas, 1 Layer, 1 Codeword case) Default =4 when 4 Antennas are selected under Uplink Cell Parameters

Default: Format 0

Double-click or use the drop-down menu to select the DCI Format for the corresponding PUSCH transmission.

See 3GPP TS 36.211, 36.212 and 36.213, for more information.

Activate DMRS with OCC

Choice: On | Off

Default: On

Double-click or use the drop-down menu to set the Activate-DMRS-with OCC parameter on or off for the corresponding PUSCH transmission.

See 3GPP TS 36.211 and 36.331, for more information.

3. DM-RS NPUSCH Settings

Multi-Tone Base Sequence Auto Calculation

Choice: Off | On

Default: On

Double-click or use the drop-down menu to turn automatic calculation for base sequence index parameter on or off.

On: Automatically calculate Base Sequence Index

Off: Manual input is available.

This parameter is only available when Number of Subcarriers in Resource Unit (N_RU_sc) is 12 or 6 or 3 (multitone). Otherwise disable with read-only.

Multi-Tone Base Sequence Index (u)

Range: 0 to 29 (maximum value depends on Number of Subcarriers in Resource Unit)

Default: 0

Enter a value for Multi-Tone Base Sequence Index (u).

It is used for DM-RS NPUSCH when group hopping is not enable.

This parameter is only available when Multi-Tone Base Sequence Auto Calculation is Off, Number of Subcarriers in Resource Unit (N_RU_sc) is 12 or 6 or 3 (multitone) and Group Hopping is Off.

Otherwise automatically decided (multitone) or disable with read-only (singletone).

See 3GPP TS 36.211 10.1.4.1.2 for more information.

Cyclic Shift (alpha)

Range:

0 to 2 (N_RU_sc = 3)

0 to 3 (N_RU_sc = 6)

0 (N_RU_sc = 12)

Default: 0

Enter a value for Cyclic Shift (alpha).

This parameter is only available when Number of Subcarriers in Resource Unit (N_RU_sc) is 12 or 6 or 3 (sigletone). Otherwise disable with read-only.

See 3GPP TS 36.211 10.1.4.1.2 for more information.

Group Hopping

Choice: On | Off

Default: Off

Double-click or use the drop-down menu to set Group Hopping on or off for DM-RS NPUSCH.

This parameter is only available when NPUSCH Format 1. Otherwise disable with read-only.

See 3GPP TS 36.211 10.1.4.1.3 for more information.

Group Assignment NPUSCH (Delta_SS)

Range: 0 to 29

Default: 0

Enter a value for Group Assignment NPUSCH (Delta_SS).

This value is used to calculate the sequence-shift pattern for DM-RS NPUSCH.

This parameter is only available when Group Hopping is On and NPUSCH Format 1. Otherwise disable with read-only.

See 3GPP TS 36.211 10.1.4.1.3 for more information.

4. UL CoMP Settings

UL CoMP State—UL-SCH

Choice: On | Off

Default: Off

Double-click or use the drop-down menu to turn the state On or Off.

 

On

 

PUSCH ID and DMRS PUSCH CSH ID are available to set a value

 

Off

 

PUSCH ID and DMRS PUSCH CSH ID are read only

See 3GPP TS 36.211 and 36.311 for more information.

UL CoMP State—UCI

Choice: On | Off

Default: Off

Double-click or use the drop-down menu to turn the state On or Off.

 

On

 

PUCCH ID is available to set a value

 

Off

 

PUCCH ID is read only

See 3GPP TS 36.211 and 36.311 for more information.

PUSCH ID

Range: 0 to 509

Default: 0

Coupling: Read only value unless UL CoMP State is set to On

Enter a value for the PUSCH Identity (ID) that is used for the virtual cell ID.

See 3GPP TS 36.211 and 36.311 for more information.

PUCCH ID

Range: 0 to 509

Default: 0

Coupling: Read only value unless UL CoMP State is set to On

Enter a value for the PUCCH Identity (ID) that is used for the virtual cell ID.

See 3GPP TS 36.211 and 36.311 for more information.

DMRS PUSCH CSH ID

Range: 0 to 509

Default: 0

Coupling: Read only value unless UL CoMP State is set to On

Enter a value that is used in the initialization of the cyclic shift hopping for the generation of the DMRS PUSCH pseudo random sequence. This is used for the virtual cell ID.

See 3GPP TS 36.211 and 36.311 for more information.

4. Transmission Settings (NB IoT)

Data

Use the data source selection dialog box to select PN9, PN15 or user defined bits to use for the data in the transport block.

This parameter is only visible when NPUSCH Format 1.

MCS Index

Range:

0 to 12 (N_RU_sc > 1 and N_RU = 1 or 2 or 3 or 4)

0 to 11 (N_RU_sc > 1 and N_RU = 5)

0 to 10 (N_RU_sc > 1 and N_RU = 6)

0 to 7 (N_RU_sc > 1 and N_RU = 8)

0 to 6 (N_RU_sc > 1 and N_RU = 10)

0 to 10 (N_RU_sc = 1)

Default: 0

Double-click or use the drop-down menu to set the MCS Index.

This parameter is only visible when NPUSCH Format 1.

See 3GPP TS 36.213 16.5.1.2 Table 16.5.1.2-1 and 16.5.1.2-2 for more information.

Modulation

Displays NPUSCH modulation type.

See 3GPP TS 36.211 10.1.3.2 for more information.

TBS Index

Displays NPUSCH TBS Index which is determined by MCS Index.

This parameter is only visible when NPUSCH Format 1.

See 3GPP TS 36.36.213 16.5.1.2 for more information.

Transport Block Size

Displays NPUSCH Transport Block Size which is determined by MCS Index and Number of Resource Units.

This parameter is only visible when NPUSCH Format 1.

See 3GPP TS 36.36.213 16.5.1.2 for more information.

RV Index Configuration

Choice: Auto | Manual

Default: Auto

Double-click or use the drop-down menu to set the RV Index Configuration.

If the RV Index Configuration is set to Auto, the RV index is automatically set in order from the first element of RV index sequence.

If the RV Index Configuration is set to Manual, User can set RV index by manual in the UL-SCH Tx sequence window.

This parameter is only visible when NPUSCH Format 1.

RV index sequence is only visible when RV Index Configuration is Auto.

RV Index Sequence

Range of sequence length: 1 to 16

Range of each value:0 or 2

Default: 0,2

Enter the numbers of individual RV Index Sequence, separated by commas.

For example, '0,2'.

Only numbers or comma inputs are allowed.The number less than or equal to 1 is rounded to 0. Others are rounded to 2.

This parameter is only visible when NPUSCH Format 1.

RV index sequence is only visible when RV Index Configuration is Auto.

See 3GPP TS 36.213 16.5.1.2 for more information.

Transmission Configuration Length

Displays the length of each UL-SCH or UCI transmission configuration.

Even though Transmission Configuration Length is set longer than Waveform Generation Length, the waveform time length is Waveform Generation Length.

Transmission Configuration

Click the button in this cell to open the UL-SCH Tx sequence window or the UCI Tx sequence window.

NPUSCH Starting Subframe

Range: 0 to Waveform Generation Length - 1

Default: 0

Enter a value of NPUSCH Starting Subframe.

NPUSCH transmission is delayed from the beginning of waveform by adding gap period.

5. Transmission Settings

Coding State

Choice: Off | On

Default: On

This parameter applies only to UL-SCH channels.

Double-click or use the drop-down menu to turn coding for the selected channel off or on.

If the Number of HARQ Processes is set to 3 or 4, the Coding State is set to On as read-only.

Data (1)

Use the Data Source Selection dialog box to select PN9, PN15, or User Defined Bits or user defined bits to use for the data in the transport block 1 (codeword 0).

See 3GPP TS 36.211, 36.212 and 36.213, for more information.

Data (2)

This parameter applies only to UL-SCH channels.

Use the Data Source Selection dialog box to select PN9, PN15, or User Defined Bits or user defined bits to use for the data in the transport block 2 (codeword 1).

See 3GPP TS 36.211, 36.212 and 36.213, for more information.

Data Reset

Choice: None | Every Subframe

Default: None

Sets the data reset method for UL-SCH.

None: the transport data is continuously repeated seed data which is specified by Data parameter. The transport data is not reset till end of waveform.

Every Subframe: the transport data is reset at the start of each subframe.

If Number of HARQ Processes is 3 or 4, Data Reset is set to None as read-only.

If UE Type is BL/CE, Data Reset is set to Every Subframe as read-only.

For eMTC Uplink CC, this parameter is set to Every Subframe first as an exception.

RB Size Restriction

Choice: On | Off

Default: On

Double-click or use the drop-down menu to turn the PUSCH Resource Block Size Restriction on or off.

If it is On, PUSCH Resource Block Size is restricted equal to (2^(a*2)) * (2^(b*3)) * (2^(c*5)) or less than RB UL max. (a, b, c is non-negative integer).

This resource restriction is according to the 3GPP standard specification.

Otherwise it is just equal or less than RB UL max. (RB UL max is system RB size)

See 3GPP TS 36.211 for more information.

Number of HARQ Processes

Choice: 3 | 4 | 8

Default: 8

Double-click or use the drop-down menu to select the number of HARQ Processes. This parameter applies only to UL-SCH channels.

This value decides the number of available hybrid automatic repeat request (HARQ) processes and defines the interval (number of subframes) between retransmissions. Use the Assigned Processes parameter to enable HARQ processes.

3 : TTI Bundling = On and e-HARQ-Pattern = On (MEU Option U05 or greater only)

4 : TTI Bundling = On and e-HARQ-Pattern = Off (MEU Option U05 or greater only)

8 : TTI Bundling = Off

If the Number of HARQ Processes is set to 3 or 4, TTI Bundling is set to On (Bundling operation).

If the Number of HARQ Processes is set to 8, TTI Bundling is set to Off (Normal operation).

Click the button in the Transmission Configuration parameter to view the enabled HARQ processes in the UL-SCH Tx sequence window.

If UE Type is BL/CE, Number of HARQ Process is set to 8 as read-only.

See 3GPP TS 36.213, 36.321 and 36.311 for more information.

Assigned Processes

Range: 0 to (number defined in Number of HARQ Processes)

Default: 0 to 7

This parameter applies only to UL-SCH channels.

Enter the numbers of individual HARQ processes, separated by commas (for example, 1,2,3) or a range of HARQ processes ( for example, 1-3) to enable specific HARQ processes. The number of available HARQ processes is defined in the Number of HARQ Processes cell.

Your setting is displayed in the UL-SCH Tx sequence window (see Transmission Configuration).

Initial RV Index

Range: 0 to 3

Default: 0

Enter the initial RV index for BL/CE UE.

This parameter appears only when UE Type is set to BL/CE.

When CE Mode is set to Mode B, this parameter is set to 0 as read-only.

See 3GPP TS 36.213 for more information.

RV Index Configuration

Choice: Auto | Manual

Default: Auto

Double-click or use the drop-down menu to set the RV Index Configuration.

If the RV Index Configuration is set to Auto, the RV index is automatically set in order from the first element of RV index sequence.

If the RV Index Configuration is set to Manual, you can set RV index manually in the UL-SCH Tx sequence window.

If the Number of HARQ Processes is 3 or 4, the RV Index Configuration is set to Auto as read-only.

This parameter appears only when UE Type is set to Non-BL/CE.

RV Index Sequence

Range of sequence length: 1 to 16

Range of each value: 0 to 3

Default: 0,2,3,1

Enter the numbers of individual RV Index Sequence, separated by commas (for example, 1,2,3).

In the case that Number of HARQ Processes is 8 (TTI Bundling is off) and RV Index Configuration is 'Manual', RV Index Sequence is read-only.

If the Number of HARQ Processes is 3 or 4, the RV Index Sequence is set to 0,2,3,1 as read-only.

Resource Block Assign

This parameter applies only to UCI channels. Select a resource block assignment for the UCI from the drop-down list. Your selection is applied to the UCI in the first slot of each subframe. The UCI in the second slot of each subframe is adjusted accordingly. Your setting is displayed in the resource mapping graph at the bottom of the Channel Setup window.

Transmission Configuration Length

Range:

Non-BL/CE: 10 ms to Waveform Generation Length, Max 160 ms

BL/CE: 1 ms (Fixed)

Step: 10 ms

Default: 10 ms

This value is set same value of Transmission Configuration Length in UL-SCH as read-only automatically.

For eMTC Uplink CC, this parameter is set to 1 ms first as an exception.

UI parameter couplings:

If the Waveform Generation Length parameter is set less than the Transmission Configuration Length, the value of Transmission Configuration Length is changed to be ≤Waveform Generation Length. In summary, the relation between Transmission Configuration Length and Waveform Generation Length is that the Transmission Configuration Length ≤Waveform Generation Length. Refer to the Waveform Generation Length parameter.

Channel

Transmission Configuration Length

Default Value

UL-SCH

The value is available to set 1 -16 Frames With following rule:

Transmission Configuration Length ≤Waveform Generation Length

10 ms

UCI

The value is automatically set to same value corresponding UL-SCH.

Same as UL-SCH

Example: Where the Transmission Configuration Length is set to 20 ms (2 frames), Frames #0 and #1 configurations (Sequences #1 through #20) will be repeated while generating ClosedSCH.

Transmission Configuration

Select an uplink channel, then click the button in this cell to open the UL-SCH Tx sequence window, or the UCI Tx sequence window.

Number of ACK bits

Displays the total number of ACK bits on the definition of UCI Transmission Configuration as generated by the PUCCH Wizard.

Number of NACK bits

Displays the total number of NACK bits on the definition of UCI Transmission Configuration as generated by PUCCH Wizard.

6. PUSCH Config Dedicated

HARQ-ACK Offset Index

Range: 0 to 15

Default: 0

Enter a value for the HARQ-ACK Offset Index. The table below shows the relationship between the HARQ-ACK offset value and the HARQ-ACK Offset Index:

0

2.000

1

2.500

2

3.125

3

4.000

4

5.000

5

6.250

6

8.000

7

10.000

8

12.625

9

15.875

10

20.000

11

31.000

12

50.000

13

80.000

14

126.000

15

reserved

RI Offset Index

Range: 0 to 12

Default: 0

Enter a value for the RI Offset Index. The table below shows the relationship between the RI offset value and the RI Offset Index:

0

1.250

1

1.625

2

2.000

3

2.500

4

3.125

5

4.000

6

5.000

7

6.250

8

8.000

9

10.000

10

12.625

11

15.875

12

20.000

13

reserved

14

reserved

15

reserved

CQI Offset Index

Range: 2 to 15

Default: 2

Enter a value for the CQI Offset Index. The table below shows the relationship between the CQI offset value and the CQI Offset Index:

0

reserved

1

reserved

2

1.125

3

1.250

4

1.375

5

1.625

6

1.750

7

2.000

8

2.250

9

2.500

10

2.875

11

3.125

12

3.500

13

4.000

14

5.000

15

6.250